Accurate insight despite foam buildup
Automatic feed of defoamer in wastewater thanks to Heartbeat Technology
ARA Worblental is relying on state-of-the-art technology in its new sludge dewatering system. The centrate water, a byproduct of the dewatering process, has a strong tendency to foam, which can lead to overflowing. To date the foam is measured with two different level sensors. With Heartbeat Technology, the process can now be efficiently monitored with just a single sensor.
Customer benefit
Foam or buildup detection during the process
Reduced maintenance effort
Lower operation costs
Higher system availability
Customer challenge
The centrate water produced by the dewatering process contains high levels of ammonium-nitrate. As a result, it can be fed into the wastewater only in doses and is thus buffered in a retention tank. Monitoring is essential since the resulting foam in the media strongly impacts the process. There is also a risk of the foam rising out of the centrate water shaft, flooding the dewatering infrastructure and causing it to back up all the way to the decanter.
State-of-the-art instrumentation
The Micropilot FMR60 radar measures the fill level of the centrate water and is able to detect the development of foam with Heartbeat Technology. Thanks to the instrument’s two power outputs, this can occur simultaneously. The second power output regulates the defoaming pumps continuously so that only so much is fed as is really necessary.
If the radar sensor detects no foam, the pumps then run at a low level.
-
Стандартные продукты
- Надежность, прочность и неприхотливость
Технический уровень
Простота
-
Высокотехнологичные продукты
- Функциональность и удобство
Технический уровень
Простота
-
Специализированные продукты
- Для требовательных областей применения