Выполните поиск по ключевым словам, коду изделия, коду заказа или серийному номеру, например: «CM442» или «Техническое описание»
Для начала поиска введите минимум 2 символа.
  • История

Singapore’s bunkering industry breaks new ground

Metcore relies on Endress+Hauser’s innovative Master Meter Solution

The bunkering industry has stringent accuracy requirements, as the margin of error in custody transfer applications is razor thin: even a 0.5% error would amount close to a whopping USD 95 million in losses. As a marine solutions provider and an authorized verifier for mass flow meter, Singapore-based Metcore sought a solution that meets the highest accountability requirements set by local authorities and international standards.

Metcore and Endress+Hauser gathered around a master meter proving skid credit: Manifold Times

Testing of the master meter skid by employees of Metcore and Endress+Hauser

An Endress+Hauser master meter proving skid in front of a Singapore bunker tanker at the port Credit from Manifold Times

Performance verification test of the mass flowmeter (MFM) unit installed aboard a Singapore bunker tanker using an Endress+Hauser Master Meter Solution

The results

  • Much faster verification operation compared to traditional master meter systems

  • Minimization of the overall downtime of the duty meter on board the bunker vessel

  • Longer uptimes and reduced overall costs thanks to a maintenance-free system without moving parts

Metcore company logo

Endress+Hauser is our competent partner with profound know-how. Their master meter proving solution enriches the bunkering industry in Singapore reducing the time and resources needed.

Darrick Pang, Managing Director
Metcore (Singapore)

The challenge

In Singapore, more than 200 mass flow meters (MFM) are installed aboard the bunker vessels, safely monitoring nearly USD 19 billion worth of transactions. With so much at stake and the bunkering industry's demanding requirements for validating the performance of duty meters, something special was needed to ensure the continuity of the bunker custody transfer operations. Given the challenges presented by the application, meter verification with a master meter was the only viable option.

Our solution

Endress+Hauser provided Metcore with an innovative master meter system that allows for easy, quick and reliable proving (calibration) of duty meters directly on site. The system – offered as a compact skid – combines high-performance Coriolis flowmeters with a flow computer. With traceable Coriolis mass flowmeter verification, Metcore was able to enhance the credibility and reputation of Singapore as a major international port.